Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
NEC Electronics (TSE 6723) today announced the availability of six new 8-bit All FlashTM microcontrollers (MCUs) with built-in CEC (consumer electronic control) controller and embedded flash memory. The new products enable interdependent control of digital audio/video (AV) applications such as digital TVs and Blu-rayTM disc players, and include three 48-pin variants, named 78K0/KC2-C and three 64-pin variants, named 78K0/KE2-C.
The new chips target the rapidly growing digital AV market. They are designed for use in devices such as flat-panel TVs and Blu-ray disc players.
NEC Electronics expects annual sales of flat-panel TVs and Blu-ray disc players to increase in the mid-term, by 17%, reaching 200 million units by 2012, and by 58%, reaching 35 million units by 2012, respectively.
Reducing power consumption is important both to meet the growing consumer demand for environmentally friendly products and to comply with environmental regulations. In the European Union, PCs, digital AV equipments and other electronic devices will be required to consume no more than 1 to 2 watts in standby mode starting from January 2010.
Many AV devices support the High-Definition Multimedia Interface (HDMI), a standard interface that allows digital AV devices to exchange audio, video, and control signals through a single cable. High-end devices will also support CEC, which promises to control AV components that support the HDMI standard. For example, when a user presses the playback button on a Blu-ray disc player, the disc player can automatically turn on a digital TV and display the playback picture via the CEC interface.
Until now, system designers needed to use their custom software to ensure connectivity between the system and multiple AV components. In this method, a host CPU must be powered on and running in order to monitor the state of the device and wait for CEC and remote control signals.
NEC Electronics' new MCUs with on-chip CEC controllers allow the CPU to be powered off during standby mode and speed up CEC and HDMI certification process while reducing power consumption and the need to develop custom software.
The main features of the new MCUs as follows.
NEC Electronics believes these new MCUs can help designers meet the demand for environmentally-friendly products, enhance the user experience, and ease the system design of AV applications of home entertainment and intends to further expand its lineup of CEC MCUs for the digital AV market.
Pricing and availability
Samples of the new MCUs will be available starting from November 2009. Pricing varies depending on memory capacity, package, and number of pins. For example, 78K0/KE2-C MCU with 60 KB of Flash memory and 3 KB of RAM equipped on a QFP package with 64-pins is priced at U.S. $ 4 per unit. Mass production of these new products is scheduled to begin in June 2010, and is expected to reach a monthly production of 2,000,000 units by September 2010. More information about NEC Electronics' extensive MCU product offerings can be found at here
(Pricing and availability are subject to change without notice.)
Please refer to the separate sheet for the main specifications of the new MCUs.
NEC Electronics Corporation (TSE: 6723) specializes in semiconductor products encompassing advanced technology solutions for the high-end computing and broadband networking markets; system solutions for the mobile handset, PC peripheral, automotive and digital consumer markets; and multi-market solutions for a wide range of customer applications. NEC Electronics Corporation has subsidiaries worldwide including NEC Electronics America, Inc. and NEC Electronics (Europe) GmbH. More information about NEC Electronics worldwide can be found at www.necel.com.
Information in the press releases, including product prices and specifications is current on the date of the press announcement, but is subject to change without prior notice.