Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
FAQ-ID : therma-nnnn
| 0001 | Basic concepts |
|---|---|
| 0002 | Modeling |
| 0003 | Thermal resistance of each part |
| 0004 | Junction temperature and thermal resistance |
| 0005 | Case examples |
| 0006 | Heat dissipation |
| 0007 | Thermal resistance of IC package |
FAQ-ID : therma-0001Last Updated : 2005/08
Potential difference = Resistance x current Temperature difference = Thermal resistance x heat (power) Thermal resistance = Temperature difference / heat (power)
FAQ-ID : therma-0002Last Updated : 2005/08
Junction: Junction temperature (Tj) | | > > Thermal resistance between a junction and case (θj-c) (°C/W) > | | Case surface: Case temperature (Tc) | | > > Thermal resistance between case and ambient air (θc-a) (°C/W) > | | Ambient air: Ambient temperature (Ta)
FAQ-ID : therma-0003Last Updated : 2005/08
FAQ-ID : therma-0004Last Updated : 2005/08
Tj = Ta + θj-a x P
Ta: Ambient temperature
θj-a: Thermal resistance between a junction and ambient air
(= between junction and case + between case and ambient air)
P: Power consumption
Based on this fact, the following can be stated
In the case of the same power consumption, the smaller thermal resistance makes smaller rise in temperature at the junction.FAQ-ID : therma-0005Last Updated : 2008/02


(2008/02)
FAQ-ID : therma-0006Last Updated : 2009/12
(2009/12)
FAQ-ID : therma-0007Last Updated : 2007/11
(2007/11)