Please note that JavaScript and style sheet are used in this website,
Due to unadaptability of the style sheet with the browser used in your computer, pages may not look as original.
Even in such a case, however, the contents can be used safely.
The following page content corresponds to the products formerly marketed by NEC Electronics
The replacement of incandescent lamps with fluorescent lamps is being promoted as a great way to reduce CO2 emissions. Consequently, the importance of fluorescent lighting is increasing and the use of inverter-controlled fluorescent lamps is becoming widespread due to their emissions efficiency. To create a highly efficient ballast lighting control system, we recommend the use of an 8-bit microcontroller capable of half-bridge and PFC control for lighting purposes - and a power MOSFET.
This combination also supports communication control by means of a digital addressable lighting interface(DALI).
* PFC: Power Factor Correction
Microcontroller
|
High-withstandvoltage power MOSFET
|